Operator Display authenticate users via user name and password.
The system administrator creates a user account with your needed permissions so you can access Operator Display and perform your assigned tasks. For more information, see Logging on to Operator Display .
There are three different types of users in Operator Display:
A building manager who has complete access to the configuration of the Operator Display, including user administration.
A maintenance person or janitor who uses the Operator Display to interact with devices without being able to modify the configuration.
A security guard who can view Operator Display features like alarms, but is not authorized to perform actions.
The minimum number of characters and how many lowercase, numeric, and special characters that are required when you create a password depends on how the Operator Display user settings are configured.
When you change your password, the password requirements for the Operator Display are displayed on the Change password screen. For more information, see Changing Password .
The following special characters can be used:
!*#$%'()*+-/:;<=>?@[\]^_'{|}~
As an administrator you add and delete user accounts, and configure user settings, such as password minimum requirements.
For more information, see User Account Administration .