earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Alarms
Product version: 2024, 7.0
10/30/2025

User Actions

arrow1_rotationAlarm Comments arrow1_rotationCause Notes arrow1_rotationAction Notes arrow1_rotationChecklists

User actions are used to ease the understanding of what triggered the alarms and what to do to solve the cause of the alarm. User action can be mandatory or optional depending on how the system is set up.

Alarm Comments

You can add a comment to an alarm that can be helpful the next time the same alarm is triggered.

For more information, see Alarm Comments .

Cause Notes

A cause note is a predefined note that contains information on what triggered the alarm. This information can be helpful the next time the same alarm is triggered.

For more information, see Cause Notes .

Action Notes

An action note is a predefined note that contains information on what you have done to solve the problem that triggered the alarm.

For more information, see Action Notes .

Checklists

Checklists are predefined lists with steps you take to correct the cause of the alarm.

For more information, see Checklists .

  • How Alarms Work
  • Alarm Comments
  • Cause Notes
  • Action Notes
  • Checklists