Reports Server is an add-on to Enterprise Server that enables advanced reporting capabilities. The Reports Server helps visualize performance using data collected from StruxureWare Building Operation and ensures that our customers make the most of their energy.
A SmartStruxure solution has the capacity to collect large amounts of data. Turning that data into information is critical to ensure that each site is running as efficiently as possible.
The StruxureWare Building Operation Reports Server is able to process large amounts of data and produce meaningful reports to facilitate analysis and optimization of each installation. The Reports Server comes with several built-in reports that meet the standard reporting needs for most installations. Other reports are available on the Schneider Electric SmartStruxure solution community site.
The Reports Server software is installed on a Microsoft Windows based computer. The Reports Server can be installed on the same computers as the Enterprise Server. Users access the Reports Server through WorkStation and WebStation or the reports-only user interface called WebReports. WebReports is designed for users who are interested in reports only. This web interface is also used for administrative tasks.
The Reports Server is built on Microsoft SQL Server. Once the data is replicated from the Enterprise Server, the reports are generated using the full potential of the off-the-shelf Microsoft technology. Standard tools, such as Microsoft Report Builder or Visual Studio, can be used for engineering to ensure an affordable and richly featured solution.
Reports or sets of reports can be downloaded from the Schneider Electric web site, or exported from existing installations. This functionality saves significant programming time when installations have similar reporting needs. It is also an opportunity for installers to provide value-added services.
To help track a facility’s performance over time, administrators can create reports that track recurring events, and store the results on the server in a popular format such as PDF, Microsoft Word, or Excel.
One way to use the reporting solution is for users to access the already generated, scheduled reports. A better way, which offers more use power, is to use the dedicated WebReports web interface. WebReports allows administrators to manage scheduled reports and report packs. In WebReports, as well as through integrated functions in WorkStation and WebStation, users can view reports, save in various popular formats, and create dashboard reports.
Reports can be created to prompt users for input before generation. This make the system very flexible in what is reported on, but sometimes it is handy to preconfigure answers to the questions. These dashboard reports are immediately run when users open them.
The image management function enables the system administrators to easily upload new logos or images to the system. This ensures that all reports are branded appropriately for each site. Further customization can also be done using a report editor.
The built-in reports meet the reporting requirements of most installations. Standard RDL (Report Definition Language) tools, such as Microsoft’s Report Builder, can be used to modify the built-in reports or to create new ones. The database itself contains the documentation of the meaning of each table, so that it is easier to create new reports or build upon the existing samples.
Energy object tagging provides building managers with finer granularity in view and characterization of their energy usage. This tagging is enabled using the Enterprise Server.
When configuring site and meter objects, tags can be attached that enables energy data categorization in custom energy reports. Assignment of multiple tags allows tracking of energy consumption by both area and usage. The system provides the user with the ability to have user defined tags, and also the following predefined tags:
Enclosed Area
Open Area
Common Area
Rented Area
Heating
Cooling
Lighting
Water Heating
Ventilation
The following factory supplied reports are part of the installation package:
Activities Per Server Report
Activities Per User Report
Alarm Amount by Category Report
Alarm Amount by Type Report
Alarms Per Server Report
Current Alarms Report
Most Active Alarms Report
System Errors Per Server Report
Top Activities Report
Top Alarms Report
Top System Errors Report
Trend Log Comparison Report
User Logins Report
Users and Groups Report
The following reports are available in the StruxureWare Building Operation Energy Reporting Pack:
Energy Monitoring Calendar Consumption Report provides an interactive report that shows the energy usage on one or multiple selected days
Energy Monitoring Consumption Breakdown Report shows energy consumption broken down using sub-metering
Energy Monitoring Consumption Report shows the energy consumption against a specified target value
| Hardware requirements | |
Processor
|
Minimum: 2 Core @ 2.00 GHz
|
Recommended: 4 Core @ 3.00 GHz or higher
|
|
Memory
|
Minimum: 4 GB
|
Recommended: 8 GB or higher
|
|
Hard disk space
|
Minimum: 20 GB
|
Drive
|
DVD drive is required if your copy of StruxureWare Building Operation was delivered on disc.
|
| For more information on hardware requirements for installing SQL Server 2008 R2, see | |
| https://msdn.microsoft.com/en-us/library/ms143506(v=sql.105) . | |
| For more information on hardware requirements for installing SQL Server 2012, see | |
| https://msdn.microsoft.com/en-us/library/ms143506(v=sql.110).aspx/html . | |
| Software requirements | |
Operating systems
|
Microsoft Windows 7 (32-bit), English
|
Microsoft Windows 7 (64-bit), English
|
|
Microsoft Windows 8.1 (32-bit), English
|
|
Microsoft Windows 8.1 (64-bit), English
|
|
Microsoft Windows 10 (64-bit), English
|
|
Microsoft Windows Server 2008 R2 (64-bit), English
|
|
Microsoft Windows Server 2012 (64-bit), English
|
|
Microsoft Windows Server 2012 R2 (64-bit), English
|
|
| The following Microsoft Windows 7 edition is supported: English edition of Professional. | |
| The following Microsoft Windows 8.1 editions are supported: English editions of Pro and Enterprise. | |
| The following Microsoft Windows 10 editions are supported: English editions of Pro and Enterprise. | |
| The following Microsoft Windows Server 2008 R2 editions are supported: English editions of Standard, Web, Enterprise, Datacenter, and Itanium. | |
| The following Microsoft Windows Server 2012 edition is supported: English edition of Standard. | |
| The following Microsoft Windows Server 2012 R2 editions are supported: English editions of Datacenter and Standard. | |
SQL versions
|
Microsoft SQL Server 2008 R2 (64-bit) SP2 or SP3, English
|
Microsoft SQL Server 2012 (64 bit)*, English
|
|
| * Microsoft SQL Server 2012 SP1, SP2 or SP3 is required if the operating system Windows Server 2012 R2 is used | |
| The following Microsoft SQL Server 2008 R2 and Microsoft SQL Server 2012 editions are supported: English editions of Standard and Express with Advanced Services. | |
Required additional software
|
Microsoft .NET Framework 4.5 or 4.6
|
| For more information on software requirements for installing SQL Server 2008 R2, see | |
| https://msdn.microsoft.com/en-us/library/ms143506(v=sql.105) . | |
| For more information on software requirements for installing SQL Server 2012, see | |
| https://msdn.microsoft.com/en-us/library/ms143506(v=sql.110).aspx/html . | |
Web browsers supported for WebReports
|
Microsoft Internet Explorer 9 (32-bit)
|
Microsoft Internet Explorer 11
|
|
Mozilla Firefox
|
|
Google Chrome
|
|
| Part number | |
| No part number for Reports Server. Reports Server license is included with purchase of the StruxureWare Building Operation Enterprise Server. | |