This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, and BACnet/IP devices. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP controller expansion modules and the DALI bus of the DALI light modules are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
This section provides recommendations on wire sizes and lengths for the Central IO modules.
For more information, see Wire Sizes and Lengths for the Central IO Modules .
This section provides recommendations on wire sizes and lengths for the AS-B servers.
For more information, see Wire Sizes and Lengths for the AS-B Servers .
This section provides recommendations on wire sizes and lengths for the RP-C controller models RP-C-12A, -12B, and -12C.
For more information, see Wire Sizes and Lengths for the RP-C-12A, -12B, and -12C Controllers .
This section provides recommendations on wires sizes and lengths for the RP-C controller model RP-C-16A.
For more information, see Wire Sizes and Lengths for the RP-C-16A Controller .
This section provides recommendations on wire sizes and lengths for the MP-C controllers.
For more information, see Wire Sizes and Lengths for the MP-C Controllers .
This section provides recommendations on wire sizes and lengths for the MP-V controllers.
For more information, see Wire Sizes and Lengths for the MP-V Controllers .
This section provides recommendations on wire sizes and lengths for the IP-IO modules.
For more information, see Wire Sizes and Lengths for the IP-IO Modules .
This section provides recommendations on wires sizes and lengths for the power input and power output (power distribution) of the RP controller expansion modules.
For more information, see Wire Sizes and Lengths for the Power Input and Power Output of the RP Controller Expansion Modules .
This section provides recommendations on wire sizes and lengths for the digital inputs of the RP controller expansion modules.
For more information, see Wire Sizes and Lengths for the Digital Inputs of the RP Controller Expansion Modules .
This section provides recommendations on wire sizes and lengths for the DALI bus of the RP controller expansion DALI light modules.
For more information, see Wire Sizes and Lengths for the DALI Bus of the RP Controller Expansion DALI Light Modules .
This section provides recommendations on wire sizes and lengths for the SMI interface of the RP controller expansion SMI blind modules.
For more information, see Wire Sizes and Lengths for the SMI Interface of the RP Controller Expansion SMI Blind Modules .
This section provides recommendations on wires sizes and lengths for the low-voltage (24 VDC) Blind outputs of the RP controller expansion blind modules.
For more information, see Wire Sizes and Lengths for the Low-Voltage (24 VDC) Blind Outputs of the RP Controller Expansion Blind Modules .
This section provides recommendations on wires sizes and lengths for the 0-10V Light outputs of the RP controller expansion light modules.
For more information, see Wire Sizes and Lengths for the 0-10V Light Outputs of the RP Controller Expansion Light Modules .
This section provides recommendations on wire sizes and lengths for the CRS-HH-REL-10 relay module.
For more information, see Wire Sizes and Lengths for the CRS-HH-REL-10 Relay Module .