earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-V
Functionalities: Hardware
Product version: 2022, 2023, 2024, 7.0
10/20/2025

RP Controller Expansion Sensor Module LED

arrow1_rotationStatus LED

There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.

 
action_zoom_plus_stroke Sensor module LED
Figure: Sensor module LED

Table: Sensor Module LED

Function

Color

Status

Red, Green

Status LED

The sensor module Status LED can be configured in the following modes:

  • Show status mode

  • Off mode

You configure the Status LED mode in the EcoStruxure Building Operation software. For more information, see Configuring RP Controller Expansion Modules .

Show status mode

The sensor module Status LED indicates the condition of the device.

Table: Sensor Module Status LED Patterns

LED Patterns

Condition

Recommended action

Green, constant

Normal operation, status OK.

No action required.

Green constant, with red flash (100 ms every 2 seconds)

Normal operation, status OK.

However, the sensor module has detected and logged an abnormal condition. When the RP controller has retrieved the diagnostics from the sensor module, the Status LED returns to constant green light. For more information, see RP Controller Expansion Module Diagnostics .

No action required.

Green, flashing (~1 Hz)

Device is starting or restarting.

No action required.

Green, flashing medium (~2 Hz)

Device is in maintenance mode. For more information, see RP Controller Expansion Module Maintenance Modes .

To exit the maintenance mode, configure a unique device address in the range supported by the RP controller model and then reset the device by disconnecting and reconnecting the device to the RP controller room bus. For more information, see Configuring the Room Bus Address for an RP Controller Expansion Sensor Module .For more information, see Connecting RP Controller Expansion Modules to an RP Controller .

Green, flashing fast (~5 Hz)

Device is initializing.

No action required.

Red, flashing (~1 Hz)

Device is non-operational due to a detected error.

Device is forced into maintenance mode.

Contact Schneider Electric Product Support Services for assistance.

Red, flashing fast (~5 Hz)

Device is inoperable due to a detected, non-recoverable error.

Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric.

Red, constant

Device is inoperable due to a detected, non-recoverable error.

Return the device to Schneider Electric.

Off mode

The sensor module Status LED is disabled.

  • RP Controller Expansion Modules
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • Configuring the Room Bus Address for an RP Controller Expansion Sensor Module
  • Connecting RP Controller Expansion Modules to an RP Controller
  • Configuring RP Controller Expansion Modules
  • RP Controller Expansion Module Diagnostics
  • RP Controller Expansion Module Maintenance Modes
  • RP Controller Expansion Sensor Module Set Button
  • RP Controller Expansion Module LEDs
  • Status LEDs
  • RP-C Models