Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP controller room bus and provide the RP controllers with I/O expansion and sensors that enable lighting and blind control.
The software application for lighting and blind control runs in the RP controller. There is typically one RP controller per room, but some RP controller models support control of up to four rooms per controller. For more information, see RP-C Models .For more information, see RP-V Models . The RP controllers are connected to an automation server, which controls and manages all the RP controllers. There is typically one automation server per floor. The automation servers are in turn typically connected to an Enterprise Server.
The RP controllers can use input data from SpaceLogic Sensor devices to control the lighting and blinds. The SpaceLogic Sensor devices are connected to the RP controller sensor bus. The SpaceLogic Sensor devices provide sensors for temperature, humidity, CO 2 , and occupancy in a room. SpaceLogic Sensor models with touchscreen display enable users to adjust the lighting and blinds in a room. For more information, see SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet .
In addition, the EcoStruxure Building Engage mobile application allows building occupants to adjust the room comfort settings (room temperature, fan speed, lighting, and window blinds) using a smartphone connected to the RP controller through Bluetooth Low Energy. For more information, see Engage .
The RP controller expansion light modules enable control of lights with electrical ballasts and LED drivers.
For more information, see Light Modules .
The RP controller expansion blind modules enable control of motorized window blinds and shutters.
For more information, see Blind Modules .
The RP controller expansion relay modules enable control of lights and motorized window blinds and shutters.
For more information, see Relay Modules .
The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.
For more information, see Sensor Modules .
The RP-C-RC-BLE remote control connects wirelessly to the RP controller expansion sensor module, such as the Multi-sensor and Insight-Sensor, and enables the occupants of modern office buildings to control the comfort level of their space.
For more information, see RP-C-RC-BLE .