The EcoStruxure Building Commission mobile application is designed to help airflow balancers, electricians, and technicians carefully and quickly pre-commission and commission SpaceLogic BACnet/IP devices, RP controller expansion modules, and EasyLogic BACnet MS/TP devices. The Commission mobile application allows light weight devices such as smartphones and tablets to be used to commission and test controllers without the need for EcoStruxure BMS servers to be connected, minimizing on-site time and reducing costs. Various checkout reports are available to confirm that the work has been done.
The Commission mobile application can connect to a single BACnet/IP controller via Bluetooth or to a network of BACnet/IP controllers on the local network, using Wi-Fi or an Ethernet cable.
The Commission mobile application does not require a license for activation and is available at no cost to the user. It is designed for use with Android, iOS (Apple), and Microsoft Windows 11 devices, and is available for download from Google Play, Apple App Store, and Microsoft Store.
After installing the Commission mobile application, users launch the mobile application by logging in with their Schneider Electric extranet credentials while connected to the internet. Once logged in, the mobile application can be used without an internet connection. Then the user cannot accidently log out until an internet connection is restored and the device running the mobile application can be used on secure sites where the device is not allowed to be connected to the internet.
The Commission mobile application provides simple workflows to perform the following for SpaceLogic BACnet/IP devices, RP controller expansion modules, and EasyLogic BACnet MS/TP devices:
Use of BACnet to discover and connect
Configure network communication settings
View status information and diagnostic files
Download application image files
Download firmware and update control via IP connection (Wi-Fi or wired)
Perform a restart
Perform checkout of inputs and outputs of a controller or an RP controller expansion module*
Perform calibration and testing of devices such as lights and blinds*
Perform commissioning of Modbus and Zigbee devices*
Quickly configure application setpoints and values with Configuration Menus
Air balance terminal boxes controlled by MP-V and RP-V controllers
Use the mobile camera device to capture controller specific data from the Data Matrix symbol on the product label and High Security Zigbee QR Codes containing IEEE Address and Install codes.
Provide feedback direct from the mobile application
* For applications with SpaceLogic BACnet/IP devices.
The user can download firmware to multiple BACnet/IP devices over an IP connection. This is useful when an application image is associated with a newer firmware version than what is currently loaded into the controller.
During I/O checkout, a report is generated in the device. In this report, any failed connections are identified so that they can be corrected. When checkout is complete, you can view the report in WorkStation. This report can serve as a record of checkout progress during the installation of a project.
With SpaceLogic RP controllers, the user can perform I/O checkout on the RP controller room bus to verify proper communication over the room bus between the RP controller and the associated RP controller expansion modules. Module type mismatches or address mismatches can then be resolved. After wiring the physical inputs and outputs of the RP controller expansion modules, the user can perform the following tasks on the different modules:
DALI light modules: discover, wink, and associate DALI lights and input devices to logical software points, and test individual lights
0-10V light modules: test individual lights
Blind modules: calibrate and test blinds
Relay module: test outputs
The user can commission Modbus devices and determine their online/offline status.
In applications with SpaceLogic RP controllers, the user can commission Zigbee devices by joining them either to a standard security, high security or VingCard network, associating them with controller objects and determine their online/offline status.
You can choose from several different options to connect the Commission mobile application to one or more BACnet/IP devices.
With SpaceLogic Bluetooth Adapter, the Commission mobile application can connect to a BACnet/IP device through Bluetooth. You plug the adapter into the side of a SpaceLogic Sensor connected to the controller's sensor bus. For more information, see the SpaceLogic Sensors - SXWS Sensors for MP and RP IP Controllers - Specification Sheet.
With the Commission mobile application, you can connect directly to an RP controller through the controller's onboard Bluetooth connectivity. By default, the controller advertises its name, model name and unique serial number. For more information, see the RP-C and RP-V Specification Sheets.
The Commission mobile application can also connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network, using a Wi-Fi router or a wireless access point.
A mobile device running the Commission mobile application can be connected to a single BACnet/IP device or to a network of BACnet/IP devices on the local network using an Ethernet cable.
| Commission mobile application | |
| Hardware and software requirements | |
Hardware
|
Android phones and tablets
|
Apple iPhones and iPads
|
|
PCs, laptops, and tablets running Microsoft Windows 11
|
|
Operating systems
|
Android 8.
1
(Oreo) and later
|
Apple iOS 11.2 and later
|
|
Microsoft Windows 11
|
|
| Compatibility | |
MP controller communication
|
|
EcoStruxure Building Operation
|
version 2.0.1 and later
|
RP-C communication
|
|
EcoStruxure Building Operation
|
version 3.0.1 and later
|
Configuration Menu support
|
|
EcoStruxure Building Operation
|
version 3.0.1 and later
|
Bluetooth connectivity
|
|
EcoStruxure Building Operation
|
version 3.0.2 and later
|
RP controller expansion module support
|
|
EcoStruxure Building Operation
|
version 3.1.1 and later
|
RP-V communication
|
|
EcoStruxure Building Operation
|
version 4.0.1 and later
|
MS/TP communication via Bluetooth connectivity
|
|
EcoStruxure Building Operation
|
version 4.0.1 and later
|
EasyLogic RP-V communication
|
|
EcoStruxure Building Operation
|
version 4.0.3 and later
|
EasyLogic RP-C, MP-C, and RP-IO communication
|
|
EcoStruxure Building Operation
|
version 5.0.1 and later
|
| IP connection security | |
| Having a secured IP connection to the site is the responsibility of the user. | |
| SpaceLogic Bluetooth Adapter | |
| Electrical | |
DC input power consumption
|
Maximum 0.25 W
|
DC input supply voltage
|
5.0 to 5.5 VDC (powered by the SpaceLogic Sensor)
|
| Communications | |
Wireless communications
|
Bluetooth
®
4.2 Low Energy compliant
|
Bluetooth
®
5 Advertising
|
|
Frequency: 2.4 GHz
|
|
Line-of-sight range: max. 50 m (164 ft)
|
|
SpaceLogic communications
|
RS-485, proprietary Sensor Bus protocol
|
| Operation environment | |
Ambient temperature, operating
|
0 to 50 °C (32 to 122 °F)
|
Ambient temperature, storage
|
-40 to +70 °C (-40 to +158 °F)
|
Humidity
|
Maximum 95 % RH non-condensing
|
| Mechanical | |
Dimensions
|
70 W x 32 H x 12 D mm (2.8 W x 1.3 H x 0.5 D in.)
|
Weight
|
0.02 kg (0.05 lb) with lanyard
|
| Agency compliances | |
EMC
|
EN 301 489-1 V2.2.0; EN 301 489-17 V3.2.0; EN 55032:2012; EN 55035:2017; FCC Part 15, Subparts B and C, Class B; ICES-003, Class B
|
Radio
|
EN 300 328 V2.2.0
|
Safety standards
|
BS/EN 62368-1:2014; BS/EN 62311:2008; BS/EN 62479:2010
|
FCC ID
|
QOQ11
|
ISED certification number
|
IC: 5123A-11
|
| Hardware | |
CPU type
|
ARM Cortex-M4 single-core
|
Frequency
|
38.4 MHz
|
SRAM (embedded)
|
32 KB
|
Flash memory (embedded)
|
256 KB
|
Flash memory (serial)
|
1 MB
|
Status indicator
|
LED (blue)
|
Button
|
Momentary push-button switch
|
| Compatibility | |
Commission mobile application
|
|
EcoStruxure Building Operation
|
version 3.1.1 and later
|
BACnet/IP Controller communication
|
|
EcoStruxure Building Operation
|
version 3.0.2 and later
|
| Part numbers | |
SpaceLogic Bluetooth Adapter
|
SXWBTAECXX10001
|