earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022, 2023, 2024, 7.0, 7.1
1/13/2022

Add Schedule Event Screen

Use the Add schedule event screen to select the type of schedule event.

 
action_zoom_plus_stroke Add schedule event screen
Figure: Add schedule event screen

Table: Add Schedule Event Screen

Component

Description

Weekly

Tap to open the Add weekly event screen, where you add a new weekly event. For more information, see Add Weekly Event Screen .

Single date exception

Tap to open the Add single date exception event screen, where you add a new event on a specific day. For more information, see Add Single Date Exception Screen .

Date range exception

Tap to open the Add date range exception event screen, where you add a new event on a specific series of dates. For more information, see Add Date Range Exception Screen .

Calculated exception

Tap to open the Add calculated date exception event screen, where you add a new event on specifically calculated dates. For more information, see Add Calculated Date Exception Screen .

Calendar exception

Tap to open the Add calendar exception event screen, where you add a new monthly event. For more information, see Add Calendar Exception Screen .

If the Calendar exception button is gray instead of blue, and you see No calendars found next to it, this option is unavaible for the moment on this device because at least 1 configured calendar is required.

  • Schedule Handling
  • Weekly Events
  • Exception Events
  • Schedules Screen
  • Add Weekly Event Screen
  • Add Single Date Exception Screen
  • Add Date Range Exception Screen
  • Add Calculated Date Exception Screen
  • Add Calendar Exception Screen