earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: RP-C, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-V
Functionalities: Hardware
Product version: 2022, 2023, 2024, 7.0
10/20/2025

Sensor Modules

arrow1_rotationRP-C-EXT-IS-BLE arrow1_rotationRP-C-EXT-MS-BLE

The RP controller expansion sensor modules can be used, for example, for infrared motion detection and luminosity measurement.

The sensor modules are available in different models with different sets of sensors that provide support for various sensor features.

Module

People Counting

Motion Detection

Luminosity Measurement

Sound Pressure Level Measurement

Temperature and Humidity Measurement

RP-C-EXT-IS-BLE

yes

yes

yes

yes

yes

RP-C-EXT-MS-BLE

no

yes

yes

no

no

RP-C-EXT-IS-BLE

The RP-C-EXT-IS-BLE Insight-Sensor connects to the RP controllers and is used for people counting, infrared motion detection, and luminosity and sound pressure level measurements, and supports Bluetooth Low Energy based applications such as beaconing and remote control communication.

For more information, see RP-C-EXT-IS-BLE .

RP-C-EXT-MS-BLE

The RP-C-EXT-MS-BLE multi-sensor connects to the RP controllers and is used for infrared motion detection and luminosity measurements. The multi-sensor supports Bluetooth Low Energy based applications such as beaconing and remote control communication. ​

For more information, see RP-C-EXT-MS-BLE .

  • Hardware Overview
  • RP Controller Expansion Modules
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • People Counting
  • Motion Detection
  • Luminosity Measurement
  • Sound Pressure Level Measurement
  • Temperature and Humidity Measurement