Two compatible ports can be connected by a binding. Bindings connect the input port of one Function Block object to the output port of another Function Block object.
An input port can have only one incoming binding, but an output port can be bound to multiple input ports. A binding can be created from an input port to an output port or vice versa. When creating a binding starting from an output port, ensure that there are no previous bindings on the input port (input ports can have only one source binding). You can redirect a binding from an already bound output to a new input port. Bindings are always created within a single Canvas.
Basic bindings (i.e., a binding directly connecting two ports) can either be done manually or automatically. To avoid having the binding lines extend across the screen, you can use remote bindings . You can convert a basic binding into a remote binding.
This feature requires EcoStruxure Building Operation version 4.0.2 or later.
You can convert a remote binding into a basic binding.
To make it easier to distinguish bindings from each other, the connections are color coded based on their data type. You can also choose the shape of your binding. You select one type of binding for the program.
Curve - bindings displayed as a simple Bézier curve between bound ports.
Orthogonal - bindings drawn with right angels between each line segment.
Straight - bindings displayed as a straight line between bound ports.
It is possible to change the binding style for a program at any time. For more information, see Changing the Binding Style .
This feature requires EcoStruxure Building Operation version 4.0.3 or later.
Orthogonal bindings will snap to the binding grid (smaller than the block grid) to facilitate the placement of parallel lines. This is not supported when using Classic Editor Style.
If a component is created that has two or more bindings to the same source outside the component, only one input port will be created for that source, instead of one for each binding.
This feature requires EcoStruxure Building Operation version 4.0.2 or later.
When creating a remote binding, remote binding blocks are given a default label of "RN" (R1, R2, etc.), where N is a consecutive index that makes the label unique. This label can be changed by the user. The names of both the source and destination remote binding blocks are always the same (i.e., renaming one will change the name of the other).
If multiple remote bindings are coming out of a single output port, they are displayed in the drop-down list visible when you scroll over the reference button link button. Related blocks are displayed with their full name (i.e., module and label) in alphabetical order. This order cannot be changed manually. Clicking on the reference button will display the target block (if it is not already visible) and select the block and the input port of the block belonging to the binding.
When a Function Block object is added using the Create New Object dialog box, some bindings are performed automatically.
introduction to this concept