earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 3.0, 3.1, 3.2, 3.3, 2022
3/20/2025

Converting CRT or CER files

You must convert any CRT or CER files to PEM. BMS only supports PEM format.

Show More
action_close

Use this workflow to purchase, convert and install server certificates.

Related information can be found in the sections after the flowchart.

 
action_zoom_plus_stroke Server certificate workflow
Figure: Server certificate workflow
Configure the DNS name for the BMS server

You must configure the DNS name for the BMS server to prevent the certificate from being locked down to a specific IP.

Install OpenSSL

Download and install OpenSSL.

OpenSSL is a software library for applications that secure communications over computer networks against eavesdropping or need to identify the party at the other end.

OpenSSL is used when you generate a Certificate Signing Request (CSR). OpenSSL is also used when converting CRT or CER files to PEM files.

Generate a Certificate Signing Request (CSR)

Before you can order an SSL Certificate, you will need to generate a CSR if you want to generate your private key yourself.

The CSR contains information, for example, common name, organization, and country, that the Certificate Authority (CA) will use to create your certificate. It CSR also contains the public key that will be included in your certificate and is signed with the corresponding private key.

For more information, see Generating a Certificate Signing Request (CSR) .

Purchase the CA certificate

Purchase SSL certificate through a certificate authority. Provide the created CSR to the certificate authority.

You then receive the certificate in CRT, CER or PEM format.

Convert CRT or CER files to PEM files

BMS only supports PEM format. You must convert all CRT or CER files to PEM.

For more information, see Converting CRT or CER files .

Add the Certificate

Add the certificate to the BMS server.

For more information, see Adding a Certificate .

Verify the Connection

Verify that the connection to WebStation is secure by accessing the BMS server via HTTPS.

To converting CRT or CER files
  1. Open SSL using the Command Prompt.

  2. Type "openssl x509 -in certFileName.cer -outform PEM -out convertedCertFileName.pem"

  • Certificates
  • Server Certificate Workflow
  • Generating a Certificate Signing Request (CSR)
  • Converting CRT or CER files