A number of software and features need licenses.
Refer to the document Part Number Summary and Hardware Software Matrix for software and features that need licenses, available on Schneider Electric Extranet.
Information regarding licenses can also be found on the specification sheets:
WorkStation For more information, see WorkStation .
WebStation For more information, see WebStation .
AS-P For more information, see SpaceLogic AS-P .
AS-B For more information, see SpaceLogic AS-B .
Edge Server For more information, see Edge Server .
Enterprise Central For more information, see Enterprise Central .
Enterprise Server For more information, see Enterprise Server .
Information on which licenses that are available for EcoStruxure Fire Operation are found in the specifications:
WorkStation For more information, see WorkStation .
WebStation
FDP server
Enterprise Central For more information, see Enterprise Central .
Enterprise Server For more information, see Enterprise Server .