Use the Consumption signature configuration interface to configure and edit the consumption signature.
Component |
Description |
|
[ Pointer ] Click to activate the pointer tool an inspect a specific value on the signature curve. |
|
[ Add regression line ] Click to add a regression line that match all points in the selected range on the dependency axis. |
|
[ Add points ] Click to add a point. |
|
[ Move points ] Click to select and move a point. |
|
Remove points Click to select and remove a point. |
Consumption |
Click to configure the axis for consumption. |
Dependency |
Click to configure the axis for dependency. |
|
[ Zoom to fit ] Click adapt the signature to the area. |