earth_america
user_standard Logga in
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Koncept

Koncept


Produkter: AO-8, AO-V-8, DI-16, DO-FA-12, DO-FC-8, AS-P, PS-24V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-4 v2, UI-8/AO-V-4, UI-8/AO-V-4 v2, UI-8/DO-FC-4, UI-8/DO-FC-4 v2
Funktionaliteter: Maskinvara
Produktversion: 3.3, 2022, 2023, 2024, 7.0
2025-08-22

Terminal Bases

arrow1_rotationBackplane Board arrow1_rotationDevice Addressing arrow1_rotationDevice Installation arrow1_rotationI/O Bus

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).

There are three different types of terminal bases for the SpaceLogic devices:

  • PS-24V power supply: one terminal block

  • AS-P servers: no terminal block

  • Central IO module: two terminal blocks

 
action_zoom_plus_stroke Terminal base for Central IO module v2
Figur: Terminal base for Central IO module v2

The terminal bases for the AS-P servers and Central IO module have the same backplane boards, which are connecting the power bus, the address bus, and communication bus from the left bus connector to the right bus connector. A common name for these buses is the I/O bus.

 
action_zoom_plus_stroke Internal configuration of the terminal bases for the AS-P servers and Central IO module
Figur: Internal configuration of the terminal bases for the AS-P servers and Central IO module

The terminal base for the PS-24V power supplies has a different backplane board, which does not pass through the power bus input from the left connector. The PS-24V power supply supplies power to the AS-P server and Central IO modules installed to the right. The ground connection is connected from the left bus connector to the right bus connector in all terminal bases, because it is used as a common signal ground for the address bus as well as the communication bus.

 
action_zoom_plus_stroke Internal configuration of the terminal base for the power supply
Figur: Internal configuration of the terminal base for the power supply

Backplane Board

A backplane board is mounted in the terminal base for the W1 width devices. The backplane board is equipped with two 2x5-pin bus connectors, a 2x6-pin electronics module connector, address logic circuitry, and a device label.

Mer information finns i Backplane Board .

Device Addressing

Each device can detect its order in the chain of connected devices and assigns itself an address accordingly. This auto-addressing feature is provided by the terminal base backplane.

Mer information finns i Device Addressing .

Device Installation

The SpaceLogic devices with the two-piece design are designed for installation on DIN rails in a cabinet.

Mer information finns i Device Installation .

I/O Bus

The I/O bus is a common bus that delivers power, address information, and communication to all devices connected to the bus. The term I/O bus also denotes the chain of devices that are connected together.

Mer information finns i I/O Bus .

  • Hardware Overview
  • PS-24V Power Supplies
  • AS-P Servers
  • Central IO Modules
  • Central IO Modules v2
  • Backplane Board
  • Device Addressing
  • Device Installation
  • I/O Bus