earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, AS-P, WorkStation, Virtual Project Servers
Functionalities: Basic Functionality, Engineering
Product version: 2024, 7.0
2/17/2025

Duplicate Field Server from a Backup Set

You can use the Restore function to re-use the configuration data from a backup set in a new standalone field server. Rather than manually configuring your preferred field server configuration, you can save time and configure the standalone field server from a backup set.

The backup set used can originate from a field server that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

For more information, see Backup Sets .

Protocol compatibility

The restore function to re-use configuration data from a backup set is supported for all protocols supported by EcoStruxure Building Operation software, except for BACnet and b3 BACnet.

LonWorks devices Neuron IDs deleted on duplicated field server

The LonWorks devices connected to the field server are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from a field server, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new field server.

For more information, see LonWorks Device Workflows .

Password deleted on duplicated EcoStruxure BMS device

When you duplicate a SpaceLogic device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server site

To create a new field server in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new field server to the Enterprise Server and select the backup set in the Create Object Wizard.

For more information, see Creating a Field Server from a Backup Set .

Standalone field server site

You use a locally stored backup set to duplicate another field server configuration in a standalone field server. You then import the backup set to a client and restore to the new standalone field server.

For more information, see Duplicating a Field Server Using Restore  .

Duplicate Field Server from a Backup Set Workflow

Use the following workflow to duplicate a field server from a backup set.

 
action_zoom_plus_stroke Duplicate Field Server using restore flowchart
Figure: Duplicate Field Server using restore flowchart
Backup a field server

Backup a field server that has the configuration you want to use in the new standalone field server.

For more information, see Backing Up EcoStruxure BMS Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

For more information, see Saving a Field Server Backup Set to Another Location .

Log on to standalone field server

Log on to a new standalone field server.

For more information, see Logging on to WorkStation as an EcoStruxure Building Operation User .

Import backup set

Import the backup set.

For more information, see Importing a Backup Set to Field Server .

Restore field server using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone field server. The communication settings from the backup set are not duplicated.

For more information, see Duplicating a Field Server Using Restore  .

Important:

When you restore a standalone field server, you are logged off and need to log on manually after the restore is complete.

  • Restore
  • Backup Sets
  • Creating a Field Server from a Backup Set
  • Backing Up EcoStruxure BMS Servers Manually
  • Saving a Field Server Backup Set to Another Location
  • Logging on to WorkStation as an EcoStruxure Building Operation User
  • Duplicating a Field Server Using Restore 
  • LonWorks Device Workflows