earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P Smoke Control, Automation Server Smoke Control, IP-IO Smoke Control, MP-C Smoke Control, MP-V Smoke Control
Functionalities: Smoke Control
Product version: 2022, 2023, 2024, 7.0
5/11/2023

Applicable Documentation for BACnet Smoke Control System Equipment

This following applicable documentation is useful for installing the BACnet smoke control system equipment.

Table: Documents for Reference

Document Number

Document Title

F-24719-2

TAC I/A Series MicroNet BACnet Smoke-Control Systems Manual

30-3001-837

b-Link Installation Sheet

30-3001-1007

Andover Continuum UL 864 BACnet Smoke Control System Design Guide 

04-16015-0x-en

EcoStruxure BMS Smoke Control System Enclosure Guide

01-16001-xx-en

EcoStruxure BMS Smoke Control System Approved Software Revisions

04-40001-0x-en

SpaceLogic Hardware Reference Guide

02-18018-xx-en

SpaceLogic AS-P-SMK and AS-P-NLS-SMK Servers Installation Sheet

02-20041-xx-en

SpaceLogic MP-C-SMK Controller Models Installation Sheet

02-20045-xx-en

SpaceLogic MP-V-SMK Controller Models Installation Sheet

02-20046-xx-en

SpaceLogic IP-IO-SMK I/O Module Models Installation Sheet

When installing the model MNB-300, MNB-V1-2 or MNB-V2-2 controllers in a smoke control system, refer to the F-24719-2 manual for installation information.

When installing any of the b3 series controllers or b-Link Repeaters described in this guide, refer to the 30-3001-837 or 30-3001-1007 manuals for installation information.

To determine the approved software revisions for the smoke control system, refer to the 01-16001-xx-en document for more information.

The SpaceLogic Hardware Reference Guide can be consulted for additional information on the PS-24V, AS-P/AS Servers, MP-C, MP-V, and IP-IO family of IP controllers, and the family of Central IO modules.

This guide takes precedence over the other manuals in regards to the system composition, configuration, architecture and restrictions/guidelines applicable to engineering the EcoStructure BMS smoke control system.

  • Safety Information