earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2023, 2024
10/30/2025

SNMP Notification Distribution Method

SNMP alarms are typically used when the alarm receiver does not have access to the EcoStruxure Building Operation software or when a central unit, for example the IT department, wants to collect alarms from different sources in one place.

You can send notifications as SNMP traps from any EcoStruxure BMS server using SNMP version 3. The EcoStruxure BMS server can send one or many traps depending on the setting.

You configure the SNMP trap to send the notification message.

Notifications sent using SNMP trap are written to the event log.

SNMP is also used to send information regarding the status of an Automation server. For more information, see Automation Servers ..

  • Notification Distribution Methods
  • Create Notification Wizard - Configure SNMP Page
  • Automation Servers
  • Email Notification Distribution Method
  • Write to File Notification Distribution Method