Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
There are five LEDs on the front panel of the AS-B server.
 
    | Function | Color | 
| Status (AS-B) | Green/Red | 
| RS-485 Tx | Yellow | 
| RS-485 Rx | Green | 
| Ethernet 1 | Green/Yellow | 
| Ethernet 2 | Green/Yellow | 
The AS-B server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.
The LEDs indicate status of the AS-B server and the ongoing communication.
The AS-P and AS-B server Status LED indicates the condition of the device.
| LED Patterns | Condition | 
| Green, constant | Normal operation, status OK | 
| Green, flashing (~1 Hz) | Device restarting, wait | 
| Green, flashing (~10 Hz) | Device shutting down | 
| Red, constant | Detected error, attention required | 
| Red, flashing (~1 Hz) | Device operates, but a problem needs attention | 
| Red/green, flashing (~1 Hz) | Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode | 
| No light | No input power | 
The RS-485 LEDs indicate the condition of the RS-485 communication.
| LED Patterns | Condition | 
| Yellow, flashing (Tx) | Transmit data | 
| Green, flashing (Rx) | Receive data | 
The Ethernet (1 and 2) LEDs indicate the condition of the Ethernet communication.
| LED Patterns | Condition | 
| Green, flashing | 10 Mbit communication | 
| Yellow, flashing | 100 Mbit communication |