The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.
An override display unit consisting of an LCD display and five keys is provided for override control of the output channels.
The override display also enables you to perform the following actions:
View inputs and outputs
Configure inputs and outputs
The following override display model is available for use with MP-C controllers and IP-IO modules.
|
Model |
|
MP-C DISPLAY a |
MP-C controller models with “-M” in the product name do not support the override display unit (MP-C Display).
The override display has a menu-driven user interface, which facilitates overriding of the outputs, local configuration of inputs and outputs, and other tasks.
For more information, see User Experience .
You use the keys on the override display to navigate the screens of the user interface and to select options on menus and lists.
For more information, see Keys .
The basic operation of the user interface includes the following actions:
Highlight an option on a menu or list
Select an option on a menu or list
Change a value
For more information, see Basic Operation .
You use the override display to manually override digital outputs as well as analog outputs.
For more information, see Override Outputs .
Using the override display, you can view the configuration and the present values for inputs and outputs, and for outputs you can also view the override status.
For more information, see View Inputs and Outputs .
In configuration mode, you can locally configure inputs and outputs for temporary use during commissioning of the device. You can configure inputs and outputs that have not been configured through WorkStation.
For more information, see Configure Inputs and Outputs for Temporary Use .
| Display | |
Display resolution
|
128 x 64 pixels
|
Display size
|
36 W x 17 H mm (1.4 W x 0.7 H in.)
|
Display type
|
FSTN monochrome LCD, white color transflective backlight
|