earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Enterprise Server, IP-IO , MP-C, MP-V, AS-P, Virtual Project Servers, RP-C, RP-V
Functionalities: Engineering, Hardware
Product version: 2022
3/30/2023

Memory in RP and MP Controllers and I/O Modules

RP and MP controllers and I/O modules are devices that have three types of memory:

  • Flash memory: for boot loader, operating system, application software, and configuration storage

  • RAM: for runtime operation

  • FRAM non-volatile memory: for data retention in the case of power outage

You can manually back up or restore the devices to a storage location on a PC or network. For more information, see BACnet Backup and Restore

When RP and MP controllers and I/O modules are part of an EcoStruxure BMS, the configuration data automatically resides in the parent EcoStruxure BMS server. The EcoStruxure Building Operation database and the device database are synchronized to help ensure there is always one backup available that can be used to restore the device memory. Scheduled backups can provide additional protection against application and data loss. In addition, device-specific values (for example, AHU or heat pump data) are duplicated in the parent server to facilitate device replacement scenarios.

Important:

For VAV controllers, ensure you back up and save the flow balance data, as this data is not covered by the database synchronization described above.

  • MP Controller Models
  • IP-IO Modules
  • BACnet/IP Controller - RP Models
  • MP-C Controllers
  • MP-V Controllers
  • RP-C Controllers
  • RP-V Controllers
  • IP-IO Modules
  • BACnet/IP Device Firmware Management
  • Free Object System Memory Utilization in BACnet/IP Controllers
  • Application Images
  • BACnet/IP Controller Communication
  • Association Selection Workflow
  • Configure an Online BACnet/IP Controller Workflow
  • BACnet/IP Controller Diagnostics
  • Device Discovery for BACnet/IP Devices
  • BACnet/IP Controller Device Management
  • Automatic Time Sync for BACnet/IP Controllers
  • BACnet Backup and Restore
  • Backing Up Flow Balance Data