earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, AS-P, WebStation
Functionalities: Localization
Product version: 2023, 2024
10/30/2025

Time and Date Editor in WebStation

Use the Time and Date editor to configure the network time server addresses or configure time on EcoStruxure BMS servers.

 
action_zoom_plus_stroke Time and date editor
Figure: Time and date editor

Table: Time and Date Editor

Property

Description

Use external NTP server

Select Enabled to define the primary and secondary NTP server addresses for connected shadow EcoStruxure BMS server devices.

NTP Server 1

​Type the address to the primary time server to which the shadow automation server date and time object synchronizes its clock.

NTP Server 2  

Type the address to the secondary time server to which the shadow automation servers' date and time object synchronizes its clock.

Lead object 

​Enter the object that acts as the lead for this object.

NTP Server 1 Key Id

Type the ID of the authentication key for the primary time server.

NTP Server 2 Key Id

Type the ID of the authentication key for the secondary time server.

NTP Server 1 Key Value

Type the password for the primary time server.

NTP Server 2 Key Value

Type the password for the secondary time server.

Authenticate Network Time Synchronization 

Select if you want to use authenticated network time synchronizing.

Date and time

Configure the date and time if you do not want to use an external NTP server.

  • Network Time
  • Time and Date
  • Configuring Time and Date using WebStation