The Browse Objects function of the Commission mobile application creates a list of all the objects within a BACnet/IP controller. You can use this function to view and, if needed, edit the properties of any of these objects.
In the Commission mobile application, connect to the BACnet/IP controller.
On the tab bar, click Configure .
Click Browse Objects .
On the Object List page, select an object.
To filter the object list, click the Filter button, select the object types you want to view, and then click Apply .
On the Edit Properties page, view the properties and their values.
To edit the value of a property, type a new value in the text box.
Some properties in the Edit Properties dialog box are read-only, indicated with values in grayed text. Others, which display their values in black text, are writable. If the controller is hosted in a server, all the values in this dialog box are grayed, including the writable properties. In that case, unhost the controller and then edit the properties as needed.
For more information, see Cannot Edit Object Properties in Controller That Is Hosted .
If you edited any of the properties, click Save .
To return to the list of objects, click the Back arrow .