earth_america
user_standard Log on
action_search_stroke
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, IP-IO , MP-C, MP-V
Functionalities: Engineering
Product version: 2.0, 2.1
3/14/2019

Device Restart

You can use the Device Restart function of the eCommission SmartX Controllers mobile application to perform a restart of the SmartX IP controller. Two types of restart are possible, Warm Restart and Cold Restart . Most of the actions performed by these restart types are the same, except one:

  • Actions common to both types:

    • The restart instructs a BACnet device to to reboot itself.

    • The device retains all configuration data.

    • Retention of run-time data, including values, is dependent on the default or user-defined retention configuration.

    • Trend data is restored, following the restart.

  • Actions that differ between the two types:

    • Warm Restart - Activates any pending changes to the network settings, such as IP assignment and IP address.

    • Cold Restart - Does not activate any pending changes to the network settings.

For more information, see Restarting a SmartX IP Controller .

  • Technician Workflows for eCommission Application
  • Restarting a SmartX IP Controller