earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Dashboards
Product version: 3.0, 3.1, 3.2, 3.3, 2022, 2023
2/23/2024

Slideshow Properties Dialog Box

Use the Slideshow Properties dialog box to configure the dashboards you want to display in the slideshow.

 
action_zoom_plus_stroke Slideshow Properties dialog box
Figure: Slideshow Properties dialog box

Table: Slideshow Properties Dialog Box

Component

Description

Speed

Type the amount of time you want each dashboard to display.

Add

Click to add a dashboard to the slideshow.

Initial path

Click to select a dashboard.

Order

Enter the order in which the dashboard is displayed in the slideshow.

Show toolbar

Select if you want to show the toolbar.

  • How Dashboards Work
  • Slideshow