earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Hardware Installation

Hardware Installation


Products: AD v3
Functionalities: Hardware
Product version: 3.3, 2022, 2023
12/3/2022

SpaceLogic™ AD v3

Safety Information

Electrical equipment should be installed, operated, serviced, and maintained only by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

Carefully read these instructions and all information relevant for this product before trying to install it. See the list of technical literature.

Technical Literature

  • SpaceLogic and EasyLogic - Hardware Reference Guide, 04-XX001-XX-en

The technical literature and declarations of conformity can be accessed on the Schneider Electric extranet, ecoxpert.se.com. Contact your local Schneider Electric sales office for a hard copy of the documentation or for additional information.

Making the Holes in a Cabinet

 
action_zoom_plus_stroke

Installing AD v3 on a Cabinet

 
action_zoom_plus_stroke

Connecting the Earth Ground Wire

 
action_zoom_plus_stroke

Connecting the AD v3 Cable

 
action_zoom_plus_stroke

Connecting AD v3 to an Automation Server and a 24 VDC Power Supply

Notice

EQUIPMENT DAMAGE

  • Never connect AD v3 to an AC power supply.

  • Do not use the Y-shaped cable to power any USB devices other than AD v3.

Failure to follow these instructions can result in equipment damage.

 
action_zoom_plus_stroke

Configuring Kiosk Mode

  • Press the AD v3 power button.

  • From the Home screen, tap the HMI Kiosk icon.

  • Enter a password to be used for HMI Kiosk and tap Submit .

    • The password must be at least 12 characters long and include an uppercase character, a lowercase character, a digit, and a symbol. To use a shorter password, tap Use a 6-character password .

    • Each device should be configured with a strong and unique password. Do not reuse the password for multiple devices.

    • Remember the password as there is no recovery key.

  • Change the WebStation address, if required.

  • Configure the screen timeout, if required.

  • Select the WebStation shortcut to run in Kiosk mode.

  • Tap Lock & Launch .

Part Numbers

Device

Part number

AD v3 bundle
SXWADBUND10003
AD v3 cable, Y-shaped, 1.35 m (4.43 ft)
SXWADUSBC10002
AD v3 cable, Y-shaped, 2.85 m (9.35 ft)
SXWADUSBC10003

Specifications

Power input
Nominal voltage
24 VDC
 
action_zoom_plus_stroke
  
20 VDC (USB-C)
 
action_zoom_plus_stroke
  
15 VDC (USB-C)
 
action_zoom_plus_stroke
  
For information on the use of 15 VDC or 20 VDC USB-C power supply to power AD v3, contact Schneider Electric.
Typical example of 24 VDC power supply
ABLM1A24012 (Schneider Electric)
Recommended USB power supply ratings
20 VDC, 1 A (20 W)
  
15 VDC, 1.5 A (22.5 W)
Power consumption
17.3 W (0.72 A at 24 VDC)
  
17.6 W (0.88 A at 20 VDC)
  
19.0 W (1.27 A at 15 VDC)
Operation environment
Ambient temperature, operating
0 to 40 °C (32 to 104 °F)
Humidity
Maximum 95 % RH non-condensing
Mechanical
Ingress protection rating
IP 54
Plastic flame rating
UL94 V-0
Dimensions (W x H x D)
258 x 195.6 x 25 mm (10.2 x 7.7 x 1.0 in.)
Weight (excluding nut)
0.933 kg (2.056 lb)

Addendum - California Proposition 65 Warning Statement for California Residents

For the AD v3 bundle, the following warning statement applies:

 
action_zoom_plus_stroke
WARNING: This product can expose you to chemicals including lead and Diisononyl phthalate (DINP), which are known to the State of California to cause cancer, and lead, which is known to the State of California to cause birth defects or other reproductive harm. For more information go to www.P65Warnings.ca.gov

For the AD v3 cables, the following warning statement applies:

 
action_zoom_plus_stroke
WARNING: This product can expose you to chemicals including Diisononyl phthalate (DINP), which is known to the State of California to cause cancer. For more information go to www.P65Warnings.ca.gov