Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
How to How to 7/23/2021
Products: Commission, IP-IO , MP-C, MP-V, RP-C
Functionalities: Engineering, BACnet/IP devices
Product version: 3.3, 2022

Downloading a Configuration Menu to a BACnet/IP Controller

You download the Configuration Menu to the BACnet/IP controller to configure the device.

Note:

Before you can download a Configuration Menu to a BACnet/IP controller, you must download the Application Image that contains the Configuration Menu to the BACnet/IP controller. For more information, see Downloading an Image File to a BACnet/IP Controller .

Hide
Show More

Configuration Menus are a group of pre-engineered objects and values that make device commissioning faster and easier. Configuration Menus are exported and downloaded from image files. Download a Configuration Menu to a BACnet/IP controller to commission the controller.

Configure Controllers Workflow

You download an Application Image that contains a Configuration Menu to a BACnet/IP controller to configure a device. Use this workflow to implement the Configuration Menu using the Commission mobile application. Related information can be found in the section after the flowchart.

For more information, see Configure Controllers with the Configuration Menu Workflow .

Download a Configuration Menu to a BACnet/IP Controller

You download the Configuration Menu to the BACnet/IP controller to configure the device.

For more information, see Downloading a Configuration Menu to a BACnet/IP Controller .

Modify Device Properties from the Configuration Menu

After downloading the configuration menu to the controller, you view and modify the device properties from the configuration menu to complete device commissioning.

For more information, see Modifying Device Properties from the Configuration Menu .

To download a Configuration Menu to a BACnet/IP controller
  1. From the Menu , select Configuration Menu .

  2. In the Configuration Menu, change any writable property values. For more information, see Modifying Device Properties from the Configuration Menu .

  3. Select Save .

The Configuration Menu has been downloaded to the BACnet/IP controller.

Community Content

Product version

Language