earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Server, AS-P, Virtual Project Servers, RP-C, RP-C-EXT-0-10V-4-PD, RP-C-EXT-BL-2-LV-PD, RP-C-EXT-BL-4-HV-PD, RP-C-EXT-DALI-M-PD, RP-C-EXT-IS-BLE, RP-C-EXT-MS-BLE, RP-V
Functionalities: Engineering, Hardware
Product version: 2023, 2024
10/30/2025

RP Controller Expansion Module Memory

RP controller expansion modules have two types of memory, flash memory and RAM.

The flash memory is used as follows:

  • Embedded flash memory: for boot loader, operating system, application software, and configuration storage

  • NOR flash memory: for log files and default configuration storage

The RAM is used for runtime operation.

The configuration data for the RP controller expansion modules resides in the RP controller to which the devices are connected. When the RP controller is part of an EcoStruxure BMS, the configuration data for the controller and expansion modules automatically resides in the parent EcoStruxure BMS server. Any configuration changes made through the EcoStruxure Building Operation software are stored in the EcoStruxure BMS server as well as the hosted RP controller and its subsystem. This means there is always a backup available for restoring or replacing an RP controller.

Note:

Configuration changes made through a third party BACnet Operator Workstation (B-OWS) or the Commission mobile application are not automatically part of the configuration data in the EcoStruxure BMS server. You need to upload such configuration changes if you want the changes to be stored in the EcoStruxure BMS server.

Scheduled backups of the EcoStruxure BMS server can provide additional protection against application and data loss. You can also manually back up or restore an EcoStruxure BMS server to a storage location on a PC or network.  

  • RP Controller Expansion Modules
  • Light Modules
  • Blind Modules
  • Relay Modules
  • Sensor Modules
  • RP-C-EXT-DALI-M-PD
  • RP-C-EXT-0-10V-4-PD
  • RP-C-EXT-BL-4-HV-PD
  • RP-C-EXT-BL-2-LV-PD
  • RP-C-EXT-DALI
  • RP-C-EXT-0-10V-4
  • RP-C-EXT-BL-SMI-4-HV-PD
  • RP-C-EXT-BL-SMI-2-LV-PD
  • RP-C-EXT-REL-4
  • CRS-HH-REL-10
  • RP-C-EXT-MS-BLE
  • RP-C-EXT-IS-BLE
  • BACnet/IP Controller - RP Models
  • RP-C Controllers
  • BACnet/IP Device Firmware Management
  • Free Object System Memory Utilization in BACnet Controllers and IO Modules
  • Application Images
  • BACnet Controller and IO Module Communication
  • Association Selection Workflow
  • Configure an Online BACnet/IP Controller Workflow
  • BACnet/IP Controller Diagnostics
  • Device Discovery for BACnet Controllers and IO Modules
  • BACnet Controller and IO Module Device Management
  • Automatic Time Sync for BACnet Controllers and IO Modules
  • BACnet Backup and Restore