Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
Use this workflow to unify domains and to make sure all the servers have the same domain after you add an Enterprise Central to your system. Related information can be found in the sections after the flowchart.
Log on to the Enterprise Server that you want to add to the Enterprise Central. For more information, see Log on to WorkStation or WebStation .
Export the domain you want to use from the Enterprise Server. For more information, see Import and Export of User Management Solutions .
Delete the domain from the Enterprise Server to avoid conflict. For more information, see Deleting a Domain .
Log on to your Enterprise Central in order to import your domain and add the servers. For more information, see Log on to WorkStation or WebStation .
Import the domain that you want to use to the Enterprise Central. For more information, see Import and Export of User Management Solutions .
Add the Enterprise Server to the Enterprise Central. For more information, see Adding an Existing Enterprise Server to an Enterprise Central .
Add the Enterprise Server to the domain of the Enterprise Central. For more information, see Adding an Existing Enterprise Server to an Enterprise Central .
Add your automation servers to the domain of the Enterprise Server. For more information, see Assigning an Automation Server to a Domain .