earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Security
Product version: 2023, 2024
10/30/2025

Configuring an Automation Server to use 802.1X MD5 Security

You configure an automation server to use 802.1X MD5 to increase the security.

Show More
action_close

Automation servers support IEEE 802.1X security. Automation servers can be configured as supplicants on a network protected by IEEE 802.1X security.

The following IEEE 802.1X authentication methods are supported:

  • MD5

  • EAP TLS

  • Protected EAP with MSCHAPv2

Important:

When using IEEE 802.1X Security, Ethernet 2 cannot be set to switch mode.

To configure an automation server to use 802.1X MD5 security
  1. Connect to the USB device port. For more information, see Connecting to an Automation Server Using the USB Device Port .

  2. In Device Administrator, click Servers and then click the server name.

  3. Click 802.1X Security .

  4. In the 802.1X Security list, select MD5 .

  5. In the Username box, enter the username configured on the authentication server.

  6. In the Password box, enter the password configured on the authentication server.

  • Security Overview
  • IEEE 802.1X Security
  • Automation Server Device Administration
  • 802.1X Security – MD5 Tab
  • Connecting to an Automation Server Using the USB Device Port