earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Operator Display
Functionalities: Administration, User Management
Product version: 3.3, 2022, 2023, 2024, 7.0, 7.1
7/22/2021

Deleting a User

You delete a user to remove it from the list of users who can access this Operator Display.

Show More
action_close

As an administrator you add and delete user accounts, and configure user settings, such as password minimum requirements.

Notice

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

  • Always select the least privileged role necessary for the user to perform their duties.

  • Always create a unique account for each individual.

  • Do not share accounts between multiple people.

  • Consider regional privacy requirements when creating user and display names, as user names will appear in event logs.

  • Ensure user names are clearly unique to help ensure clear traceability. For example, avoid creating both “User1” and “User 1”.

Failure to follow these instructions can result in unauthorized system access or disclosure of private information.

User Account Creation

When you create a new user you need to fill in a user name, a display name, a role, and a password.

User name

The minimum number of characters for the user name is 3 and no spaces are allowed.

Display name

The minimum number of characters for the display name is 3 and no leading, trailing or consecutive spaces are allowed.

Role

Operator Display supports the management of users under three roles; Administrator, Technician, and Viewer.

Table: Secure Account Management

Tasks

Administrator

Technician

Viewer

View BACnet properties and alarms

Yes

Yes

Yes

Set/force BACnet Points

Yes

Yes

-

Acknowledge BACnet Alarms

Yes

Yes

-

View event logs

Yes

Yes

Yes

Export logs to USB

Yes

Yes

-

Change Operator Display configuration

Yes

-

-

Upgrade Operator Display firmware

Yes

-

-

Add/delete users

Yes

-

-

Password

The minimum number of characters and how many lowercase, numeric, and special characters that are required when you create a password depends on how the Operator Display user settings are configured.

For more information, see Creating a User .

User Account Configuration

The following Operator Display user settings are configurable:

Inactivity timeout

The default setting is that the user is logged out after 15 minutes of inactivity. You can configure the timeout to be between 1 and 60 minutes.

Number of failed log in attempts

The default setting is that the user is locked for 10 minutes after 5 failed log in attempts. You can configure the number of failed log in attempts to be between 1 and 10.

User lock time

The default setting is that the user is locked for 10 minutes after 5 failed log in attempts. You can configure the user lock time to be between 1 and 60 minutes.

Minimum number of password characters

The default setting is that the minimum number of password characters is 8. You can configure the minimum number of password characters to be between 4 and 128. The maximum number of password characters is always 128.

Minimum number of lowercase characters

The default setting is that the minimum number of lowercase characters is 1. You can configure the minimum number of lowercase characters to be between 0 and 128.

Minimum number of uppercase characters

The default setting is that no uppercase characters are required (0). You can configure the minimum number of uppercase characters to be between 0 and 128.

Minimum number of numeric characters

The default setting is that the minimum number of numeric characters is 1. You can configure the minimum number of numeric characters to be between 0 and 128.

Minimum number of special characters

The default setting is that the minimum number of special characters is 1. You can configure the minimum number of special characters to be between 0 and 128.

The following special characters can be used:

!*#$%'()*+-/:;<=>?@[\]^_'{|}~

Note:

Operator Display alerts you if the total number of lowercase, uppercase, numeric, and special characters exceeds 128.

For more information, see Configuring User Settings .

To delete a user
  1. In Operator Display, tap the menu button

     
    action_zoom_plus_stroke
    .

  2. On the menu, tap Settings .

  3. On the Operator Display Settings screen, tap User Administration .

  4. On the User Administration screen, tap the arrow to select a user.

  5. On the user detail screen, tap the button to delete the user

     
    action_zoom_plus_stroke
    .

  6. On the Delete User screen, tap Delete .

  • User Account Administration
  • User Administration Screen