earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Basic Functionality
Product version: 2023
2/8/2023

Creating a Stand Alone Widget using WorkStation

You create stand alone widgets in your folder structure. The stand alone widgets are used when you create dynamic widgets.

Show More
action_close

Dynamic widgets is a way to automatically add graphics to a dashboard using a search function.

You configure the dynamic widget to search for, and display, a graphic in a specific location.

The dynamic widget simplifies the configuration of a dashboard when, for example, you want to present device overviews in a dashboard, where each device is represented by a TGML graphic.

If you have TGML graphics, for example a status overview in each device folder, you can display these graphics in a dashboard using the dynamic widget, without having to browse for each graphic. In the dynamic widget, you specify the common root folder for the graphics as well as the names of the graphics. We assume that the graphics have the same name, or at least that part of the name is common. Namely, it is possible to use wildcards when specifying the name of the graphic.

When the dashboard is opened, the graphics are searched and a TGML widget is created in the dashboard for each graphic found.

It is also possible to use stand-alone widgets instead of, or together with, TGML graphic. You create stand-alone widgets in WorkStation.

To create a stand alone widget using WorkStation
  1. In WorkStation, in the System Tree pane, select the folder where you want to create the stand alone widget.

  2. Right-click and click New object .

  3. Expand Dashboard , then expand Widgets .

  4. Select the stand alone widget and then click Create .

  • Dynamic Widgets