Use the Alarm Presentation dialog box tab to configure how an alarm is presented.
|
Component |
Description |
|
Alarm message |
Type the message to display when the alarm is in Alarm state. For more information, see Alarm Messages . |
|
Alarm priority |
Enter the priority level of the alarm. For more information, see Alarm Priority . |
|
Reset message |
Type the message to display when the alarm is reset. For more information, see Alarm Messages . |
|
Category |
Enter the category the alarm belongs to. For more information, see Alarm Categories . |
|
Category 2 |
Enter the second category the alarm belongs to. For more information, see Alarm Categories . |
|
Prefix for alarm source name |
Add a substitution code or type a prefix that is added to the beginning of the source name property of an alarm record. For more information, see Alarms Substitution Codes . |
|
Disable state-change logging |
Select to prevent an alarm state change from creating an event. For more information, see Alarm State-Change Logging . |
|
Auto hide |
Select to automatically hide the alarm in the Alarms pane or Alarm View. For more information, see Alarm Decoration . |
|
Flashing alert |
Select to make the alarm row flash in the Alarms pane and Alarm Views when the alarm is triggered. For more information, see Alarm Decoration . |
|
Audible alert |
Select to make the alert audible when the alarm is triggered. For more information, see Alarm Decoration . |
|
Custom audio |
Enter the path to the custom audio file you to play when the alarm is triggered. For more information, see Custom Audible Alarm Alerts . |