Use the device detail screen to interact with the device and its features.
The device detail screen is also available without configuration menus. For more information, see Device Detail Screen (without Configuration Menus) .
|
Component |
Description |
|
Alarms |
Tap to open the Alarms screen, where you view and acknowledge alarms specific to this device. This option is only visible if alarms are configured on this device. For more information, see Alarms Screen . |
|
[Configuration Menu: Control Panel] |
Tap to open the configuration menu, a customized and simplified view of the information, where you view and edit the values. For more information, see Configuration Menus . |
|
Schedules |
Tap to open the Schedules screen, where you view and edit schedule events specific to this device. This option is only visible if schedules are configured on this device. For more information, see Schedules Screen . |
|
Trend Logs |
Tap to open the Trend Logs screen, where you view event logs specific to this device. This option is only visible if trend logs are configured on this device. For more information, see Trend Logs Screen . |
|
Device Info |
Tap to open the Device Info screen, where you view more information on the device and rediscover to refresh its inputs, outputs, and values. For more information, see Device Info Screen . |