earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Operator Display
Functionalities: Schedules
Product version: 3.3, 2022, 2023, 2024, 7.0, 7.1
4/24/2023

Edit Calendar Exception Screen

Use the Edit calendar exception screen to add, edit or delete the time span and the value of a calendar exception.

 
action_zoom_plus_stroke Edit calendar exception screen
Figure: Edit calendar exception screen

Table: Edit Calendar Exception Screen

Component

Description

Priority

Tap + or - to edit the priority of the event. 1 is the highest priority and 16 is the lowest. For more information, see Exception Event Priorities .

Calendar

Tap the pencil icon to open the Select calendar screen, where you tap the radio button next to the calendar of your choice.

Start time

Displays the starting time of the event.

End time

Displays the ending time of the event.

Value

Displays the selected value of the event.

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you add a time span and a value. For more information, see Edit Exception Event Screen .

 
action_zoom_plus_stroke

Tap to open the Edit exception event screen, where you edit the time span and the value. For more information, see Edit Exception Event Screen .

  • Schedule Handling
  • Exception Events
  • Exception Event Priorities
  • Schedules Screen
  • Add Schedule Event Screen