earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 2024, 7.0
6/11/2024

Creating a Meter Processor

You create a meter processor so that you can process and analyze the energy consumption.

Show More
action_close

You can monitor, process, and analyze energy consumption using the meter object, the meter processor object, and the consumption signature object in EcoStruxure Building Operation.

Meter Object

The meter object is used to log and calculate values from a physical meter using a point, called monitored variable, in the EBO server. The monitored variable can, for example, be a Modbus point or a BACnet point.

For more information, see Meter Object .

Meter Processor

The meter processor object is used to process the information from one or many meter objects. Using the meter processor, you can add or subtract energy consumption from many different meter objects. A meter processor can also process information from another meter processor.

For more information, see Meter Processor .

Consumption Signature

The consumption signature object is used to calculate, analyze, and graphically present expected energy consumption.

For more information, see Consumption Signature .

To create a meter processor
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server or folder where you want to create the meter object.

  2. On the File menu click New object .

  3. In the list, expand Meter .

  4. Select Meter Processor and click Create .

  5. Edit the properties.

    For more information, see Meter Processor – Basic Tab .

    For more information, see Meter Processor – Outputs Tab .
  • Energy Consumption Overview
  • Meter Processor – Basic Tab
  • Meter Processor – Outputs Tab