You replace the CMOS battery in AD v3 to be able to boot up AD v3 when the existing battery is dead.
Disconnect the AD v3 cable from the AD v3 cable fitting.
Use a Phillips #1 (PH1) screwdriver to loosen the earth ground screw.
Loosen and remove the nut from the cable fitting and then gently remove AD v3 from the cabinet.
Remove the AD v3 back cover.
Loosen the 14 screws using a Phillips #1 (PH1) screwdriver.
Remove the back cover.
Disconnect the existing CMOS battery.
Carefully unplug the female connector of the CMOS battery from the male connector on the PCBA.
Put the unplugged connector with its two wires to the side, out of the way.
Do not try to remove the disconnected CMOS battery but leave it where it is mounted on the other side of the PCBA.
Remove the release liner from the foam tape and attach the tape to the new CMOS battery.
Remove the release liner from the foam tape on the CMOS battery.
Connect the new CMOS battery.
Carefully plug the female connector of the CMOS battery into the male connector on the PCBA.
Using the foam tape, attach the CMOS battery to the integrated circuit located near the male connector on the PCBA.
Replace the AD v3 back cover.
Ensure that the gasket is properly fitted into the groove of the front cover.
Fit the back cover to the front cover.
Tighten the 14 screws using a Phillips #1 (PH1) screwdriver. Ensure that the screws are fully tightened. Use the following recommended screw tightening torque: 0.4 Nm (3.5 lbf.in).
You can now install AD v3 on the cabinet. For more information, see Installing AD v3 on a Cabinet .