Use the Type permissions view to grant user accounts or user account groups extended access to a specific type.
For more information, see Creating Type Permissions Templates .
Component |
Description |
Relative to |
Click ![]() |
Type name |
Displays the name of your type. |
![]() |
Add Click to select the object that you want to add to the permission path. |
![]() |
Delete Click to remove an object that you have added to the permission path. |
Relative object |
Displays an object or objects added to the permission path. |
Read |
Select to permit viewing and listing path content. |
Write |
Select to permit an administrator to change configurations except for bindings, programs, and graphics. |
Create |
Select to permit creating new objects on the path. |
Delete |
Select to permit deleting objects under the path. Delete permissions are required on a folder to delete its contents. |
Edit |
Select to permit editing objects on the path. |
Force |
Select to permit forcing values on the path. |
Command |
Select to permit the execution of commands on the path. Command permissions can override this permission for specific commands. |
Properties |
Click to configure properties. |