Use the Advanced Commands submenu to execute functions on the selected LonWorks device or Xenta device.
|
Command |
Description |
|
Wink |
Click to generate a response from the device, such as flashing the power LED. |
|
Clear Status |
Click to clear the diagnostic data for the device or local node. For more information, see LonWorks Device Properties – Diagnostics Tab . |
|
Warm Start |
Click to restart the device without clearing the RAM memory. For more information, see Xenta LonWorks Device Restart . |
|
Cold Start |
Click to restart the device and clear the RAM memory. For more information, see Xenta LonWorks Device Restart . |
|
Alarm Refresh |
Click to transfer all alarms buffered in the physical Xenta device to the EcoStruxure Building Operation database. For more information, see Alarms for Xenta LonWorks Devices . |