earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Server, Virtual Project Servers
Functionalities: User Management
Product version: 1.8
10/13/2016

Panel Wizard – Panel Configuration Page

Use the Panel Configuration page to add components to the panel.

 
action_zoom_plus_stroke Panel configuration page
Figure: Panel configuration page

Table: Panel Configuration Page

Component

Description

 
action_zoom_plus_stroke

Add

Click to add a new component to the panel. For more information, see Create Object Wizard – Naming the Object Page .

 
action_zoom_plus_stroke

Edit

Click to edit the properties of a component. For more information, see Pane Properties .

 
action_zoom_plus_stroke

Remove

Click to remove a component from the panel.

Work area initial path

Click to enter the path for the Work area component.

Show toolbars

Select Yes to show the toolbars for the Work area component.

  • Panel Components
  • Panel Properties
  • Create Object Wizard – Naming the Object Page