earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 2023
12/4/2024

Tools Menu

Use the Tools menu to open Control Panel or make a number of user settings.

 
action_zoom_plus_stroke Tools menu
Figure: Tools menu

Table: Tools Menu

Command

Description

Control Panel

​​Click to open the Control Panel where you get access to some of the most used administration functions, such as alarms, domains, user accounts, backup and archiving, and engineering. For more information, see Control Panel Tab .

Language

Click to open the Language submenu where you select a different WorkStation language. For more information, see Language Packages .

Measurement system

Click to open the Measurement system submenu where you select a different local measurement system. For more information, see Units .

Database mode

Click to configure WorkStation to run in database mode so changes are saved to the EcoStruxure BMS server database and not sent to any physical devices. For more information, see Database Mode .

Options

Click to open the Options dialog box where you manage some local user settings. For more information, see Options Dialog Box .

  • Control Panel Tab
  • Language Packages
  • Units
  • Database Mode
  • Options Dialog Box