earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Enterprise Central, Enterprise Server, Virtual Project Servers
Functionalities: Localization
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
11/29/2024

Configuring Enterprise Server, Enterprise Central, and WorkStation Date and Time

You adjust the date and time of an Enterprise Server, Enterprise Central, or WorkStation through the operating system where Enterprise Server, Enterprise Central, or WorkStation is installed.

Show More
action_close

​In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.

 
action_zoom_plus_stroke WorkStation displays all times as local time, according to the operating system settings on which WorkStation is installed.
Figure: WorkStation displays all times as local time, according to the operating system settings on which WorkStation is installed.

For example, a WorkStation in Athens surveys an Autmation server in New York. WorkStation in Athens has a Greek operating system, which is configured to Eastern European Summer Time (UTC +2h) with +1h DST offset. The New York Automation server triggers an alarm at 07:43 Eastern time. WorkStation instantly reports the alarm but presents the alarm with the timestamp 14:43 which is the local time in Greece.

Some features in WorkStation, such as trend log and schedule, allow you to change the displayed time to UTC or server local time.

Server Time in WorkStation

The exception in WorkStation is the Local Date & Time property for the time on an Automation server where the time is displayed in local server time and not in the perspective of WorkStation and its operating system.

To configure Enterprise Server, Enterprise Central, and WorkStation Date and Time
  1. Close all EcoStruxure Building Operation software applications.

  2. For more information on how to adjust the date and time, refer to the manufacturer’s manual for the operating system.

Note:

The time zone settings for an Enterprise Server and Enterprise Central are configured through WorkStation and not the operating system.

  • Changing an EcoStruxure BMS Server Time Zone
  • Creating an EcoStruxure BMS Server Custom Time Zone
  • Time and Time Zone Configuration in WorkStation
  • Time and Time Zone Configuration in Enterprise Server and Enterprise Central
  • Date & Time View
  • Enterprise Server does not Synchronize its Clock