Use the Function Block Program Internal Alarm Properties - Alarm Settings tab to change the alarm settings of a function block program internal alarm.
Component |
Description |
Acknowledgement type |
Select the type of acknowledgement for the alarm. |
Alarm message |
Type the message to display when the alarm is in Alarm state. For more information, see Alarm Messages . |
Reset message |
Type the message to display when the alarm is reset. |
Alarm priority |
Enter the priority level of the alarm. |
Category |
Enter the category that the alarm belongs to. |
Cause note group |
Enter the cause note group that is used by the alarm. |
Action note group |
Enter the action note group that is used by the alarm. |
Checklist |
Enter the checklist that belongs to the alarm. |
Checklist required |
Select to force the user to check each step in the checklist before the alarm can be acknowledged. |
Prefix for alarm source name |
Type a prefix that is added to the beginning of the source name property of an alarm record. |
Disable alarm |
Select to disable the alarm, for example, before deployment. |
Auto hide |
Select to automatically hide the alarm in the Alarms pane or Alarm View. |
Disable state-change logging |
Select to prevent an alarm state change from creating an event. |
Flashing alert |
Select True to make the alert flash in the Alarms pane and Alarm Views when an alarm is triggered. |
Audible alert |
Select True to make the alert audible when an alarm is triggered. |
|
Edit Click to open the property pane where you edit the selected user action. For more information, see User Action Properties . |
|
Add Click to open the Create Object: Attachment wizard, where you add an attachment. For more information, see Create Object Wizard – Naming the Object Page . |
|
Edit Click to open the property pane where you configure the attachment. For more information, see Attachment Properties . |
|
Remove Click to remove an attachment that is connected to the alarm. |