earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
10/30/2025

Xenta Central Schedule Editor

Use the Xenta Central Schedule Editor to add, view, or edit Xenta central schedules.

 
action_zoom_plus_stroke Xenta Central Schedule Editor
Figure: Xenta Central Schedule Editor

Table: Xenta Central Schedule Editor

Property

Description

Add

Click to add a new weekly event.

Interval type

Select the interval type.

Start time

Select the start time for the weekly event if Interval is selected.

End time

Select the end time for the weekly event if Interval is selected.

(Select weekday)

Select the weekdays the weekly event is to be in service.

 
action_zoom_plus_stroke

Click to delete a weekly event.

Interval type

Select the interval type.

Start date

Select the start date for the exception event interval.

Start time

Select the start time for the exception event.

End date

Select the end date for the exception event interval.

End time

Select the end time for the exception event.

(Select weekday)

Select the weekdays the exception event is to be in service.

 
action_zoom_plus_stroke

Click to delete an exception event.

  • Xenta Schedules in WebStation
  • Adding a Weekly Event to a Xenta Schedule in WebStation
  • Adding an Exception Event to a Xenta Schedule in WebStation
  • Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation
  • Editing or Deleting an Exception Event in a Xenta Schedule in WebStation