Use the Alarm Control Panel Properties to view the referenced lead object.
Property |
Description |
Lead object |
Displays the referenced lead object from which all configuration data is copied. For more information, see Lead and Shadow Relationship . |
Decimal symbol |
Select the decimal symbol to be used in the notification and the notification report template. |
Substitute missing data with |
Enter the text that is displayed when a value is missing. By default, a missing value displays nothing at all. |