The Timed Force Multistate object has a single multistate input that can be bound to another object to receive a value. The input's value is passed directly to a single multistate output, which can be bound to an object that is to be controlled. With a Timed Force Multistate object, you can select and then force the display of a text string associated with one of the states created in the object. An active timed force can be changed or cancelled as needed.
You can navigate between the available open windows in the Work area. The windows you can select using the Window menu are represented by tabs in the Work area.
In WorkStation you can customize your workspace to some extent. You can, for example, decide where workspace components, such as, Alarms are displayed.
A pane is a separate area in the workspace. You use panes to carry out commands, navigate the system or display information. Panes can be moved, hidden, closed, and repositioned.
SmartStruxure Registration Portal is an interface to register your Building Operation system. To access the registration portal, you should have Schneider Electric Buildings Exchange user account.