49 Topic(s)
Use the Operator Display Settings screen to configure Operator Display and perform administrative tasks.
You change the user regional settings in WebStation so that it fits your region.
You change the user theme settings so that it fits your screen.
You change the user theme settings so that it suits your needs.
You change the default system regional settings in WebStation so that it fits your region.
Use the Date and time tab to configure the server to use an external NTP server and to configure a time zone.
Values in the EcoStruxure Building Operation software are stored in the EcoStruxure Building Operation database with all input decimals. If a stored value consists of more decimals than the operating system is defined to display, the value is rounded off according to the operating system settings before it is displayed in WorkStation.
Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.
To adjust the automation server time, time zone, and DST, you have to access the automation server through a WorkStation.
Use the Select Unit dialog box to define the unit and metric prefix of a value.