Use the Snap To menu to edit the grid time interval for the shedule view to define how precis you can be when editing the time span of a schedule event using the drag and drop method in the Advanced Schedule Editor. The default time interval is 15 minutes.
When you create a schedule, the time zone of the EcoStruxure BMS server that contains the schedule determines the execution of the events. If the schedule is copied to an EcoStruxure BMS server in a different time zone, the specified dates and times relate to the new time zone.
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.