Touchscreen

20 Topic(s)
Use the filters below to limit the number of search hits.
Products
Display all
WorkStation
WebStation
Graphics Editor
WebReports
Script Editor
Function Block Editor
Device Administrator
​License Server
​License Administrator
Software Administrator
Enterprise Server
PS-24V
AO-8
AO-V-8
DO-FA-12
DO-FC-8
UI-16
DI-16
UI-8/AO-4
UI-8/AO-V-4
UI-8/DO-FC-4
WebHelp
Automation Server
Administrator Tools
Power Supply
Central IO Modules
Project Configuration Server
Mobile Apps
Technician Tool for iOS
Technician Tool for Android
RTD-DI-16
Support Tools
Registration Portal
Transition
TAC Vista Conversion Tool
AS-P
AD v1
Project Configuration Tool
SmartXKiosk
Automation Servers
Continuum Conversion Tool
AS-B
Automation Server Smoke Control
AS-P Smoke Control
AD v2
MP-C
MP-V
Advanced Display
Enterprise Central
SpaceLogic Sensor
eCommission SmartX Controllers
BACnet/IP Devices
RP-C
IP-IO
AD v3
HMI Kiosk
RP-C-EXT-0-10V-4-PD
RP-C-EXT-BL-2-LV-PD
RP-C-EXT-BL-4-HV-PD
RP-C-EXT-DALI-M-PD
RP-C-EXT-MS-BLE
Engage
RP Controller Expansion Modules
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
RP-C-EXT-DALI
RP-C-EXT-0-10V-4
RP-C-EXT-BL-SMI-4-HV-PD
RP-C-EXT-BL-SMI-2-LV-PD
RP-C-EXT-REL-4
RP-C-RC-BLE
RP-C-EXT-KNX
Zigbee Adapter
CRS-HH-REL-10
Touch Screens
Operator Display
Builder for Function Block
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
SpaceLogic Sensor Modular Bases and Covers
SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.
5/16/2022
SpaceLogic Sensors
SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.
1/25/2022
SpaceLogic Sensor Touchscreen Display Model
The Touchscreen Display model provides a menu-driven interface with a front menu and a functions menu screen that you configure through EcoStruxure Building Operation.
12/17/2021
Selecting the Degree Type
In the SpaceLogic Sensor Touchscreen Display model, you select the degree type in order to see the temperature in the preferred units of the room occupant. You enable this feature by choosing the Display object Allow temperature unit changes property, followed by the Temperature units property and its Fahrenheit or Celsius option.
7/23/2021
Selecting the Fan Speed
In the SpaceLogic Sensor Touchscreen model, you select the fan speed to change the air flow in the designated living space. You enable this feature using the Display object Allow fan speed changes property.
7/23/2021
Selecting the Scenes Menu
You can program lighting control to create special scenes that illuminate an area based on the time of day, such as dimming the lights with the click of the night light button.
7/23/2021
SpaceLogic Sensor Models
SpaceLogic Sensor include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.
7/23/2021
SpaceLogic Sensor Touchscreen Display Model- Front Menu Screen
Use the SpaceLogic Sensor Touchscreen Display model front menu screen to view and change the current settings and advance to the functions menu screen.
7/23/2021
SpaceLogic Sensor Touchscreen Display Model- Functions Menu Screen
Use the SpaceLogic Sensor Touchscreen Display model functions menu to perform a variety of tasks. For example, with the functions menu configured as shown, you can perform the following tasks:
7/23/2021
SpaceLogic Sensor Touchscreen Display Model- Integrator Menu Pages
When allowed, you use the SpaceLogic Sensor Touchscreen Display model integrator menu pages to access information about the on-board sensors, the sensor device itself, the parent RP Series controller, and custom text messages.
7/23/2021

Product version

Language