earth_america
user_standard Log on
action_search_stroke
earth_america

AD v3

Refine your search
arrow2_down
Refine your search

14 Topic(s)

Specifications

Specifications

How to

You replace the CMOS battery in AD v3 to be able to boot up AD v3 when the existing battery is dead.

Concept

This section provides safety information specific to AD v3. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.

How to

You connect AD v3 to a SmartX server in order to communicate with the SmartX server over a wired (USB) connection. You connect AD v3 to a 24 VDC power supply in order to supply AD v3 with power. You use the Y-shaped cable (SXWADUSBC10002 or SXWADUSBC10003) to connect AD v3 to both the SmartX server and the power supply.

How to

You perform a recovery (factory reset) of AD v3 to restore the device to factory default settings.

Concept

AD v3 is installed on a control cabinet using a 22 mm (0.87 inch) cable fitting (gland) and a nut. AD v3 is delivered with the cable fitting integrated on the back cover. The position of AD v3 on the cabinet is fixed by the earth ground screw and the nut fastens the device to the cabinet.

Concept

SmartX Advanced Display v3 (AD v3) is the successor to AD v2. AD v3 provides an industrial grade Human Machine Interface (HMI), with battery-free power supply, for local access to the EcoStruxure BMS servers.

Hardware Installation

Hardware Installation