earth_america
user_standard Log on
action_search_stroke
earth_america

AO-V-8

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

37 Topic(s)

Concept

The override switches on Central IO modules with manufacturing date earlier than 2021-W26 must be disabled to remove the risk of an improper output. To disable the override switches, update the Central IO module firmware to version 2.017 or later.

Concept

For Central IO modules with outputs, the following components on the front provide control of the output channels:

Concept

The I/O wiring recommendations provide guidance on what type of wires should be used for the different Central IO modules, AS-B server onboard I/O, RP and MP controller onboard I/O, and IP-IO and RP-IO I/O modules, how to perform grounding, and how to connect different external devices to the inputs and outputs. This section also provides information on the external connectors required for the RP controller expansion modules and the RP-C-16C-F-230V model. Always use the recommended cables and wires.

Specifications

Hardware Installation

Part number: SXWTBIOW110002

Hardware Installation

Part number: SXWTBIOW110001

Hardware Installation

Part numbers: SXWDI16XX10001, SXWUI16XX10001, SXWRTD16X10001, SXWDOA12X10001, SXWDOA12H10001, SXWDOC8XX10001, SXWDOC8HX10001, SXWAO8XXX10001, SXWAO8HXX10001, SXWAOV8XX10001, SXWAOV8HX10001, SXWUI8D4X10001, SXWUI8D4H10001, SXWUI8A4X10001, SXWUI8A4H10001, SXWUI8V4X10001, and SXWUI8V4H10001

Concept

Output modules support a number of electrical types, such as digital, tristate, and digital/tristate pulsed outputs, or analog outputs. The available output modules include the following:

Concept

These Central IO modules are analog output, 8-channel I/O modules. You can use the analog outputs to control a wide range of devices, such as valves and actuators, using a 0-10 VDC control signal.

How to

You install a terminal base on a horizontal DIN rail to ensure that the device is securely fastened and to allow sufficient cooling air flow through the electronics module. You install a terminal base on a DIN rail prior to connecting it to its neighboring terminal bases.